Variable Monitoring
When your application is running:
- all variables in the Dictionary are animated 1 To better track variables and expressions of the PLC programs in Test mode, the KAS IDE dynamically computes their value along with the program execution and display the result in gray boxes beside their usage in the instruction lines of the IEC 61131-3 editor. with real-time values displayed in the Value column (see call out
) - a specific column is used to indicate the initial values of all variables

Figure 5-72: Variable Dictionary
See Also
|
Copyright © 2018 Kollmorgen |
|